REGEN.TEST
Description
This command is used to trigger the self-test to ensure the regen resistor has been wired correctly.
Executing REGEN.TEST will put current through the regen resistor circuit and verify bus voltage drops by a percentage (REGEN.TESTVTHRESH) of the initial voltage. If the timeout, (REGEN.TESTTO), is exceeded the test will fail.
REGEN.TESTSTATUS shows the results of the test. If the bus voltage reaches the threshold before the timeout, everything is considered correct and the test passes. If a short circuit is present, the test will fail early, and a fault will be present. If an open circuit is present, the test timeout will be surpassed, and the failure is reported in the test status.
Versions
|
Action |
Version |
Notes |
|---|---|---|
|
Implemented |
02-07-03-000 |
|
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
|
See Also |
|
|
Stored in Non-Volatile Memory |
No |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
REGEN.TEST |
3007h |
07h |
Unsigned32 |
- |
- |
Write only |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
2406 |
1 |
2406 (0x966) |
REGEN.TEST |
Unsigned8 |
Read/Write |
No |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
REGEN.TEST |
2406 |
Unsigned8 |
Read/Write |
- |